Technical FAQs

Ask a Question

What is the Degree of protection for iQuick PRD.

The Degree of protection for iQuick PRD is:
 Device Only                           : IP20,IK05
 Device in modular enclosure : IP40
Was this helpful?
What can we do to improve the information ?