Technical FAQs

Ask a Question

Can I communicate Vijeo Citect with Moxa Convertor (like 5150) to read data from energy meters.

To communicate with this Moxa device you need to use the Modbus protocol in Vijeo Citect. You need to create a virtual com port in moxa device and use that com port for communication with Vijeo Citect. Attached some Vijeo Citect configuration settings, INI parameters & Moxa Settings for your reference.
Was this helpful?
What can we do to improve the information ?