Technical FAQs

Ask a Question

In SRC6KUXI ,We need to know its capacity to supply surges and overloads at its output for the very short, short and medium term (such as for 10 Cycles, 10 Seconds and 2 Minutes).

Kindly find the details below : Overload capacity-102 % continuous, 103% -125% for  1 minute, 150% - 30 seconds , Above 150% 25 cycles 

Short circuit- 25 cycles maximum.
Was this helpful?
What can we do to improve the information ?