Technical FAQs

Ask a Question

Can I show Vijeo Citect`s trend data into tabular form.

You can show the trend data into tabular form by using some of the following inbuilt functions to extract trend data in excel, csv or dbf file from Vijeo Citect :

TrnExportCSV

TrnExportDBF

TrnExportDDE

Note : Details on these inbuilt functions will be provided in help file, but using these functions there will be a limitation of 8 tag export.

Also there is utility Trend Reader available that can help you to read trend data . Trend Reader displays all the header fields and data from a trend file. You can display HST files or data files from either 2-byte or 8-byte trends from any Vijeo Citect release up to and including v7.x.

Run Citect Trend Reader and click the Help button for more information.
Was this helpful?
What can we do to improve the information ?