Technical FAQs

Ask a Question

How to Set the Coldstart Delay for the Rack PDU in AP86** models ?

Path: Configuration > RPDU > Device
The Coldstart Delay is the number of seconds added to each outlet’s Power On Delay before an
outlet will turn on after power is applied to the Rack PDU. Allowed values are from 1 to 300 seconds,
Immediate, or Never (never turn on).
1. Make a selection for Coldstart Delay.
2. Click Apply.
Was this helpful?
What can we do to improve the information ?