Technical FAQs

Ask a Question

How to Reset Peak Load and kWh in AP86** model ?

Path: Configuration > RPDU > Device
1. Click the Configuration tab, then RPDU, then Device.
2. Click the Peak Load and Kilowatt-Hours check boxes as desired.
3. Click Apply.
Was this helpful?
What can we do to improve the information ?