Technical FAQs

Ask a Question

How to Create a global outlet group in AP86** model ?

Path: Configuration > RPDU > Switched Outlet > Outlet Groups
To set up multiple global outlet groups that link to outlet groups on other Rack PDUs:
1. Make sure outlet groups are enabled. (See “Typical outlet group configurations” on
page 96.)
2. Click Create Global Outlet Groups.
3. Select the checkboxes of the outlets that will be in the group and then click "Apply and
Select Global Outlets" to select the global outlet for the group. If there is only one
outlet in the group, it will automatically be assigned as the global outlet.
4. To add outlets to any of the global outlet groups you created, see “Edit or delete
an outlet group” .
Was this helpful?
What can we do to improve the information ?