Technical FAQs

Ask a Question

How to Edit or delete an outlet group in AP86** model ?

Path: Configuration > RPDU > Switched Outlet > Outlet Groups
1. In the Configure Group table, click on the number or name of the outlet group to edit or
delete.
2. When editing an outlet group you can do any of the following:
– Rename the outlet group.
– Add or remove outlets by clicking the checkboxes to mark or unmark them.
Note: You cannot remove an outlet from an outlet group that contains only two outlets
unless the remaining outlet is a global outlet.
3. To delete the outlet group, click Delete Outlet Group
Was this helpful?
What can we do to improve the information ?