Technical FAQs

Ask a Question

What is the value of Electro Static Discharge Resistance(ESD) for XB4 range of products.

For this XB4 range the Electrostatic Discharge Resistance (ESD) is 8 Kv in free air (in insulating parts) and 6 KV on contact (on metal parts) as per the IEC 61000-2-6 standard.Attached a catalogue page for reference.
Was this helpful?
What can we do to improve the information ?