Technical FAQs

Ask a Question

What is the main difference between the controllers XD2GA84217 and XD4PA24.


This XD2 is our old product range is it is replaced with XD4 range. Apart from the dimension this XD4PA** is having the actuation angle of 30 deg in each direction as compared to the XD2GA** which is having 40 deg actuation angle in each direction.
Was this helpful?
What can we do to improve the information ?