Technical FAQs

Ask a Question

Which version of Vijeo Citect SCADA is compatible with Windows 8.1 operating system.

At the time Vijeo Citect version 2015 is compatible with Windows 8.1 operating system.
Also you can use Vijeo Citect 7.20 version with Service Pack 5 installed/upgraded with Windows 8.1 operating system.
Was this helpful?
What can we do to improve the information ?