Technical FAQs

Ask a Question

What is the threshold voltage when the drive Altivar 71 switches on the braking transistor.


When drive is regenerating, the drive switches on the braking transistor when the value of bus voltage is superior at threshold voltage.
If the value of the bus voltage is inferior at the same threshold, the transistor switches off.
Refer to attached file for voltage value: The threshold is OBR.
Was this helpful?
What can we do to improve the information ?