Technical FAQs

Ask a Question

How can I get the Events log in Vijeo Citect 7.40 alarm page for any user action like when he pressed any buttons etc.

To get the details of the operator or event log in VJC 7.30 version onwards, you need to call the SOEEventAdd() from the button to log message option.
Attached a sample Vijeo Citect backup with snapshot for your reference.

When you use this SOEEventAdd() function to log the operator action you will get all the operator details on SOE page of Vijeo Citect.
Was this helpful?
What can we do to improve the information ?