Technical FAQs

Ask a Question

What is the Degree of protection for iTL Impulse relay.

The Degree of protection for iTL Impulse relay is:
Device only                             : IP20
Device in modular enclosure  : IP40 Insulation class II
Was this helpful?
What can we do to improve the information ?