Technical FAQs

Ask a Question

What is the ratio or the current rating of the primary input and the secondary output for 34035 External sensor for earth-fault protection

For this current transformer 34035 , the secondary ratio or NCT ratio is linked to frequency
* 50Hz is 221µV/A
* 55Hz is 242µV/A
* 60 Hz is 264µV/A.
Was this helpful?
What can we do to improve the information ?