Technical FAQs

Ask a Question

What’s the meaning of “controlled air” for Earthing Switch as mentioned in Premset catalogue

It means that the tank of Earthing Switch is containing only natural air at atmospheric pressure.
In the other hand, it means as well that the industrial and design of the  tank is similar to a ‘sealed for life’ tank as specified by IEC.
Was this helpful?
What can we do to improve the information ?