Technical FAQs

Ask a Question

is Premset compact metering M06S complying with international standards

Yes, M06S is compliant with IEC 61000-4-30, IEC 61557-12,. Therefore, it passes all the routine tests specified by the standards.
Was this helpful?
What can we do to improve the information ?