Technical FAQs

Ask a Question

Is it possible to integrate non =S= control and monitoring modules in Premset C&M system

Yes, it is, because our solution is open and using standard protocols.
For example, a third party RTU can easily be connected to the system.
Was this helpful?
What can we do to improve the information ?