Technical FAQs

Ask a Question

What is the minimum current sensing of self powered VIP protection ?

The minimum current sensing without any external power supply is less than 7A.
When the current is very low, the relay is sleeping but can be awaken by fault currents in less than 10ms.
Was this helpful?
What can we do to improve the information ?