Technical FAQs

Ask a Question

Why is there a battery embedded in, VIP relays ? what is the life expectancy ?

VIP relays are totally self powered. We had to integrate a battery in order to display the indications when CB is open and without any external power.
The battery has no effect on protection itself.
Its life expectancy is more than 10 years.
Was this helpful?
What can we do to improve the information ?