Technical FAQs

Ask a Question

What is the Temperature - environmental characteristic for Premset.

Temperature (Indoor Version)
> Storage : from – 40°C° to + 80 C°
> Operation: from – 25°C to + 40°C
(normal conditions) IEC 60721 - level 3K6
> Operation: from -40 °C to -25°C or +40°C to + 55°C
 
Was this helpful?
What can we do to improve the information ?