Technical FAQs

Ask a Question

Does the VIP400/410 have inputs/outputs as per Sepam 10 ?

Yes, VIP 410 integrates an "external tripping input" for this application. The VIP 40 / 45 / 400 do not, because it is non compatible with their self-powering function.
Was this helpful?
What can we do to improve the information ?