Technical FAQs

Ask a Question

Can Timer function block be retentive in M221 controller

Yes, it is possible to configure Timer function block of M221 controller as retentive.
This feature is only supported from SoMachine Basic software version V1.4 and onwards. Compatible firmware versions of M221 for SoMachine basic V1.4 is v1.4.0.x
 
Was this helpful?
What can we do to improve the information ?