Technical FAQs

Ask a Question

Does M221 controller have sink outputs

Yes, there are 6 numbers. of M221 controller references having sink transistor outputs
- 4 controllers:  M221C16U, M221C24U, M221CE16U and M221CE24U are with sink transistor outputs
- 2 controllers:  M221C40U and M221CE40U are with sink transistor outputs and 4 PTOs.

Note: All these 6 controllers with sink transistor outputs are supported only with SoMachine Basic v1.4 and onwards.
Was this helpful?
What can we do to improve the information ?