Technical FAQs

Ask a Question

What is the number of communication scanner (input / output) in Altivar Process drives

Communication scanners 1 for Modbus and 1 for Ethernet are available.
Below are the limits of inputs/ outputs.

Ethernet: 32 I/O
Modbus: 8 I/O
 
Was this helpful?
What can we do to improve the information ?