Technical FAQs

Ask a Question

What would be the behavior of SoMachine v4.1 when trying to open SoMachine v3.1 project with protected POU

- V3.1 project with protected POU -> open in V4.1 without project update => project opens but POU cannot be accessed without user and password
- V3.1 project with protected POU -> open with project update => user and password required at the beginning of project opening/update. Reason: SoMachine checks all objects for user rights and tries to synchronize the old settings of user rights to the new user rights – therefore it is needed to access the POU and the password is requested.
Was this helpful?
What can we do to improve the information ?