Technical FAQs

Ask a Question

How to configure all sensors or a defined group in netbotz 200 ?

Follow this procedure to massconfigure all sensors or a defined group of sensors.
You can mass configure temperature and humidity thresholds, rate of change settings, the alarm generation
setting, and the name and location. When mass-configuring Name and Location
fields, you can use wildcards so the system creates unique names and locations based
on automatically detected data about the module to which the sensor is connected.
1. Use filter settings to display the group of sensors to mass configure. (For
information on setting filters, see Tables.)
2. Click Mass Configuration. Make selections, then click Next.3. Enter data in fields. If you chose Name or Location, include wildcard
characters4. Click Apply, then click Finish.
Was this helpful?
What can we do to improve the information ?