Technical FAQs

Ask a Question

How to do Configuring event actions by Events in Netbotz 200 ?

1. Select the Administration tab, Notification on the top menu bar, and by event
under Event Actions on the left navigation menu.
2. In the list of events, review the marked columns to see whether the action you
want is already configured. (By default, logging is configured for all events.)
3. To view or change the current configuration, such as recipients to be notified by
e-mail or paging, or Network Management Systems (NMSs) to be notified by
SNMP traps, click on the event name. NOTE :If no Syslog server is configured, items related to Syslog configuration
are not displayed.
Was this helpful?
What can we do to improve the information ?