Technical FAQs

Ask a Question

What is the type of Output connectors is used in AP7553?

Please find the Output Connector type below :20 – IEC-320-C13,
4 – IEC-320-C19 outlets
Was this helpful?
What can we do to improve the information ?