Technical FAQs

Ask a Question

Why I am getting message "An invalid range of state RAM addresses was allocated to 140_DAI_353_00 module at the \2.2\1.5 relative topological address" in Unity Pro.

This message comes when required State RAM address range are less than the allocated range. So increase the State RAM memory range as required from CPU configuration tab.
Was this helpful?
What can we do to improve the information ?