Technical FAQs

Ask a Question

How can I integrate a Pelco IP camera with Vijeo Citect SCADA.

With help of ActiveX Controls there is an easier and quicker way to embed video streams into Vijeo Citect SCADA display pages. The selection of an ActiveX control will depend on the camera and/or formatting video type that you want to play. Kindly find the attached detailed document on this with a sample Active X for your reference. In the attachment there is a Videoocx.chm help file in which under section >> How to use Video OCX >> Saving AVI Movie Files you will get some help on the required functions . I have attached 

Also attached a detailed document which clarifies the steps to configure Pelco Series camera with Vijeo Citect along with a sample OCX file for reference. 
Was this helpful?
What can we do to improve the information ?