Technical FAQs

Ask a Question

What is th Power Supply Filtering Times for M340 power supplies.

The BMX CPS 2000, BMX CPS 3500, and BMX CPS 3540T power supplies, which provide Vac power, have a filtering time of 10 ms. 
The BMX CPS 2010 and BMX CPS 3020 power supplies, which provide Vdc power, have a filtering time of 1 ms. 
Was this helpful?
What can we do to improve the information ?