Technical FAQs

Ask a Question

Describe LUFP7 Gateway.

The LUFP7 gateway allows a master located on a Profibus-DP network to enter into a dialogue with the slaves on a Modbus RTU network. This is a generic protocol converter operating in a way which is transparent to the user.
This gateway allows you to interface many products marketed by Schneider Electric with a Profibus-DP network. These include TeSys U motor starters, Altivar drivers and Altistart soft start- soft stop units.
Was this helpful?
What can we do to improve the information ?