Technical FAQs

Ask a Question

Which default modbus slave device configuration is stored into LUFP7.

LUFP7 gateways are shipped pre-configured to allow you to interface a Profibus-DP master with 8 predefined Modbus slaves (TeSys U motor starters).
Was this helpful?
What can we do to improve the information ?