Technical FAQs

Ask a Question

Explain characteristics of vigilohm fault locator XD312.

Characteristics of vigilohm XD312 fault locator as follow;
  • Operating threshold: 2,5 mA at 2,5 Hz. 
  • IMD (e.g., IM400) must be in alarm with injection boosted. 
  • Threshold reached only for low impedance faults.
Was this helpful?
What can we do to improve the information ?