Technical FAQs

Ask a Question

List typical application of IT earthing system arrangement.

Here are the typical applications of IT earthing system arrangement;
  • In hospital and marine, IT is mandatory according to the standards.
  • Some industry applications use IT to ensure that faulty current does not represent a danger of fire or explosion (munition storage, mines, silos).
  • Other industry applications use IT to ensure continuity of service (cold storage, emergency lighting, nuclear power stations, airports)
  • In Photovoltaic applications, as well, IT is used. This is growing market.
Was this helpful?
What can we do to improve the information ?