Technical FAQs

Ask a Question

List down characterisitcs of IM400 vigilohm sytem compared to XM200 vigilohm offer.

Compared to XM200, IM400 has:
  • Same cut out but only 9cm length
  • Embedded Modbus communication
  • Compatibility with the HV subassemblies for high voltage power systems
  • Compatibility with control power systems and variable speed drives
  • Compatibility with high capacitance power systems
  • Improved Metering principles (3 frequencies injected)
  • Advanced HMI
  • 8 languages
Was this helpful?
What can we do to improve the information ?