Technical FAQs

Ask a Question

What is the function of the Compact Flash memory cards and on which Magelis display units can they be used?

CF (Compact Flash) cards are used to store the following types of information:
  • historical data,
  • recipe data,
  • alarm data,
  • project backups. 

They can be used on the following target machines:
  • XBTGT2000 range, excluding XBTGT2110;
  • XBTGT4000 range;
  • XBTGT5000 range;
  • XBTGT6000 range;
  • XBTGT7000 range;
  • XBTGK range;
  • old XBTG range.
Was this helpful?
What can we do to improve the information ?