Technical FAQs

Ask a Question

How to install PCPE application ?

Back-UPS which is PCPE application compatible, cable 40-00127(rj-45 to USB connector) should be connected between UPS and the computer, run the application setup file, read the terms and conditions and accept it to finish the install process.
Was this helpful?
What can we do to improve the information ?