Technical FAQs

Ask a Question

How to select Battery type selector switch for SRC1KUXI model.

The available battery options, FLD/SMF, are provided in the rear panel.
Keep battery selector switch in suitable position as per the specific type of battery used with the UPS. 
Was this helpful?
What can we do to improve the information ?