Technical FAQs

Ask a Question

With the TSXCUSB485 cable, which Modbus driver should I install for use in Windows Vista Business Edition 32?

The Modbus 2.0 IE10 driver needed for the various Schneider programs which use the Modbus protocol (TwidoSuite, Advantys, PL7) is available in the attachment.
It supports the TSXCUSB485 USB cable and the TSXPCX1031 serial cable.
This attachment is an executable file which includes:
  • The Modbus driver
  • The USB bus Windows driver
  • The virtual serial port Windows driver
This executable is found in the Schneider V2.6+ drivers pack.
Was this helpful?
What can we do to improve the information ?