Technical FAQs

Ask a Question

What is the difference between TSXP571634 and the TSXP571634M.

The TSXP571634 and the TSXP571634M are the same Premium CPUs. They have the same specifications. The "M" at the end of the part number only indicates multi-language documentation.

For coated version add C at the end of the reference: example TSXP571634M becomes TSXP571634MC.

If Product reference is without any Suffix then no documentation will be provided with the Product.
Was this helpful?
What can we do to improve the information ?