Technical FAQs

Ask a Question

How to import an external eds file in Advantys software

Any third party device cannot be added to the Advantys catalog by importing the EDS file into the Advantys software. 
Advantys is a CanOpen bus but it is not an open bus. The modules in the catalog have be made available only after they are incorporated into a new software release. This means that any module, Advantys and Non-Advantys modules ( in the Preferred and Enhanced catalogs) are added by the development team and go through Engineering Development and Verification / Validation Testing. 
Was this helpful?
What can we do to improve the information ?