Technical FAQs

Ask a Question

What is the efficiency of ATS48 Soft Starter.

For the efficiency of ATS48 Soft Starter, it can be calculated by using the formula:---
 
Efficiency = (Pn - Loss) / Pn.
 
Pn : nominal Power.
Loss (Power dissipated at nominal load): Given in the ATS48 Catalogue
 
Example:
 
ATS48C48Q 250KW
Power dissipated 1386W
 
Efficiency at 100% Load = (250000-1386)/250000 = 99.4%
 
Same way, it is possible to calculate for other soft starters.
 
Was this helpful?
What can we do to improve the information ?