Technical FAQs

Ask a Question

What is replacement of premium module TSXP57202

TSXP57202 is not commercial for many years. It's a Premium PL7 CPU, one slot wide. TSXP57203 should be a replacement of 57202, but it's a 2 slots wide CPU. In some applications, if the Premium rack (backplane) is full it should be the problem, so check the configuration accordingly.
Was this helpful?
What can we do to improve the information ?