Technical FAQs

Ask a Question

Is there any bandwidth limitation when use the auxiliary Ethernet port from BMECRA


The Service Ports have these limited bandwidth limitations: 

BMEP58xxxx : 100 Mbps (no limit)
BMEH58xxxx : 100 Mbps (no limit)
BMXCRA312x0 : 5 Mbps
BMECRA31210 : 5 Mbps 
140CRA31200 : 5 Mbps

 
Was this helpful?
What can we do to improve the information ?