Technical FAQs

Ask a Question

Does M580 HSBY support Time stamping features

Yes, the ERT modules as well as the Timestamping in BMxCRA are supported. As well as internal variables timestamping features is also avaiable.
Was this helpful?
What can we do to improve the information ?