Technical FAQs

Ask a Question

How to set Master IP for STBNIP2311 module.

Follow the Below Step to configure the Master IP for STBNIP2311:

>> Open Adavantys Configuration software

>> Open Workspace file

>> Unlock the configuration by clicking on Key Icon on tool bar.

>> Double click on NIP module.

>> Go to Ethernet Parameters Tab

>> Click on the Enable Editing check box .

>> Go to Mater IP Tab

>> Assign the Master IP address in Master1 .For Example. PLC IP or NOE . If required we can assign upto 3 master IP with single NIP.

>> Default Resevation Time and Holdup time are 60000ms and 1000ms respectively. Change if required to customize

>> Click OK and then save the configuration 

>> Reload the new  settings to the STB.
Was this helpful?
What can we do to improve the information ?