Technical FAQs

Ask a Question

How to program Analog Output to output frequency on ATV71 drive.

There is only one Analog Output (AO1) on ATV71 drive without option card.
 
Program following in [ INPUTS / OUTPUTS CFG] (I-O-) Menu;
 
- AO1 [AO1 assignment] to [Motor freq.] (OFr): Output frequency, from 0 to [Max frequency] (tFr).
- AO1t [AO1 Type] to [Voltage] (10U): Voltage output
- UOL1 [AO1 min Output] to 0 V
- UOH1 [AO1 max Output] to 10.0 V
 
You will get 10V between AO1 & COM when Output frequency is max frequency (tFr).
 
Was this helpful?
What can we do to improve the information ?