Technical FAQs

Ask a Question

What is the service life of the RCA remote control.

The mechanical endurance of the RCA remote control is 10,000 switching cycles (O-C).
The electrical endurance varies depending on the use of the associated circuit breaker (rating, derating, class of use, pf).



 
Was this helpful?
What can we do to improve the information ?